earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface utilisateur

Interface utilisateur


Produits : Enterprise Central, Enterprise Server, Project Configuration Tool
Fonctionnalités : Localisation
Version produit : 2.0, 2.1, 3.0, 3.1, 3.2
24/10/2018

Date & Time View

Use the Date & Time view to configure shadow SmartX server network time settings, and the time zone of the Enterprise Central or Enterprise Server.

 
action_zoom_plus_stroke Date & time view
Figure : Date & time view

Table : Date & Time View

Component

Description

Network time synchronization 

Select to define the primary and secondary network time server addresses for connected shadow SmartX server.

Enable

Select to define the primary and secondary network time server addresses for connected shadow SmartX server.

Authenticate Network time synchronization

Select if you want to use authenticated network time synchronizing.

Primary time server

​Type the address to the primary time server to which the shadow SmartX server date and time object synchronizes its clock.

Secondary time server

Type the address to the secondary time server to which the shadow SmartX servers' date and time object synchronizes its clock.

Key id

Type the ID of the authentication key for the primary time server.

Key id

Type the ID of the authentication key for the secondary time server.

Key value

Type the password for the primary time server.

Key value

Type the password for the secondary time server.

Manually adjust date & time

Select to use manual date and time configuration for connected shadow SmartX server.

Disable

Select to disable all SmartX server date and time shadow relationships and use the SmartX server own date and time configurations.

Predefined time zone

​Select the time zone the EcoStruxure BMS server belongs to.

Custom time zone

Select to manually define the EcoStruxure BMS server time zone.

Description

Type a description or name for the customized time zone DST settings.

UTC offset

Select the time difference the time zone has from UTC in the hours and minutes boxes.

This custom time zone uses daylight saving time

Select to enable the daylight saving time settings for the custom time zone.

Time adjustment

​Select the time adjustment, in minutes, for the daylight saving time.

Month - Start

Select the month that daylight saving time starts.

Week - Start

​​Select the week of the month that daylight saving time starts.

Day - Start

Select the day of the week that daylight saving time starts.

Time - Start

Select the time that daylight saving time starts.

Month - End

Select the month that daylight saving time ends.

Week - End

Select the week that daylight saving time ends.

Day - End

Select the day of the week that daylight saving time ends.

Time - End

Select the time that daylight saving time ends.

  • Time and Time Zone
  • Time and Time Zone Configuration in Enterprise Server and Enterprise Central
  • Synchronize Network Time Settings
  • List View Toolbar
  • Device Discovery View
  • Communication View