Produkty: Enterprise Server, Software Administrator
Funkcje: Podstawowa funkcjonalność, Aktualizacja
Wersja produktu: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2017-03-22

Server Installation Wizard – Configuration Page

Use the Configuration page to configure the port number the Enterprise Server listens to when communicating through a specific protocol.

 
action_zoom_plus_stroke Configuration page
Rysunek: Configuration page

Tabela: Configuration Page

Component

Description

HTTP Port

​Type the port number that the Enterprise Server listens to when communicating through the Hypertext Transfer Protocol.

HTTPS Port

Type the port number that the Enterprise Server Server listens to when communicating through a secure version of the Hypertext Transfer Protocol.

TCP Port

Type the port number that the Enterprise Server listens to when communicating through the Transmission Control Protocol.

  • Installing the Enterprise Server
  • Repairing the Enterprise Server
  • Reinstalling the Enterprise Server
  • Upgrading the Enterprise Server
  • Configuring the Value Transfer Interval
  • Software Administrator