earth_america
user_standard 登录
action_search_stroke
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2024, 7.0
2024/12/3

Enumeration Alarms

​An enumeration is a variable with labeled values; different variables have different enumerations. When configuring an enumeration alarm, you configure the variable and its enumerations to monitor.

For example, you create an enumeration alarm that monitors the reliability variable of an I/O point. The alarm is configured to trigger when the reliability variable has an enumeration that indicates the value generated by the I/O point is unreliable.

Enumeration alarms can be configured using shunt variable and time delay. 有关更多信息,请参阅 Alarm Functions .

  • Alarm Types
  • Alarms Overview
  • Alarm Functions
  • Enumeration Alarm Properties – Basic Tab
  • Creating an Enumeration Alarm