An enumeration is a range of values representing a specific command or event.
The following tables list the enumeration values for the supported alarm and event properties.
The table lists the enumeration values for Alarm State.
Enumeration value |
Enumeration definition |
0 |
Normal |
1 |
Alarm |
2 |
Acknowledged |
3 |
Reset |
4 |
Disabled |
5 |
Fault |
The table lists the enumeration values for Alarm State.
Enumeration value |
Enumeration definition |
0 |
Unassigned |
1 |
Assigned |
2 |
Accepted |
The table lists the enumeration values for BACnet Alarm Type.
Enumeration Value |
Enumeration definition |
0 |
Change of bitstring |
1 |
Change of state |
2 |
Change of value |
3 |
Command failure |
4 |
Floating limit |
5 |
Out of range |
6 |
Complex event type |
8 |
Change of life safety |
9 |
Extended |
10 |
Buffer ready |
11 |
Unsigned range |
The table lists the enumeration values for Basic Evaluation State.
Enumeration value |
Enumeration definition |
0 |
False |
1 |
True |
The table lists the enumeration values for Disabled Cause.
Enumeration value |
Enumeration definition |
1 |
Shunt variable |
2 |
User |
4 |
System |
The table lists the enumeration values for Evaluation State.
Enumeration value |
Enumeration definition |
0 |
Normal |
1 |
Off-normal alarm |
2 |
Upper limit alarm |
3 |
Lower limit alarm |
4 |
Life safety alarm |
5 |
Faulty alarm |
The table lists the enumeration values for Hidden.
Enumeration value |
Enumeration definition |
0 |
False |
1 |
True |
The table lists the enumeration values for Previous Alarm State.
Enumeration value |
Enumeration definition |
0 |
Normal |
1 |
Alarm |
2 |
Acknowledged |
3 |
Reset |
4 |
Disabled |
5 |
Fault |
The table lists the enumeration values for System Alarm ID. Für weitere Informationen siehe System Alarm ID Enumerations .
The table lists the enumeration values for System Event ID. Für weitere Informationen siehe System Event ID Enumerations .