An enumeration is a range of values representing a specific command or event.
The following tables list the enumeration values for the supported alarm and event properties.
The table lists the enumeration values for Alarm State.
|
Enumeration value |
Enumeration definition |
|
0 |
Normal |
|
1 |
Alarm |
|
2 |
Acknowledged |
|
3 |
Reset |
|
4 |
Disabled |
|
5 |
Fault |
The table lists the enumeration values for Alarm State.
|
Enumeration value |
Enumeration definition |
|
0 |
Unassigned |
|
1 |
Assigned |
|
2 |
Accepted |
The table lists the enumeration values for BACnet Alarm Type.
|
Enumeration Value |
Enumeration definition |
|
0 |
Change of bitstring |
|
1 |
Change of state |
|
2 |
Change of value |
|
3 |
Command failure |
|
4 |
Floating limit |
|
5 |
Out of range |
|
6 |
Complex event type |
|
8 |
Change of life safety |
|
9 |
Extended |
|
10 |
Buffer ready |
|
11 |
Unsigned range |
The table lists the enumeration values for Basic Evaluation State.
|
Enumeration value |
Enumeration definition |
|
0 |
False |
|
1 |
True |
The table lists the enumeration values for Disabled Cause.
|
Enumeration value |
Enumeration definition |
|
1 |
Shunt variable |
|
2 |
User |
|
4 |
System |
The table lists the enumeration values for Evaluation State.
|
Enumeration value |
Enumeration definition |
|
0 |
Normal |
|
1 |
Off-normal alarm |
|
2 |
Upper limit alarm |
|
3 |
Lower limit alarm |
|
4 |
Life safety alarm |
|
5 |
Faulty alarm |
The table lists the enumeration values for Hidden.
|
Enumeration value |
Enumeration definition |
|
0 |
False |
|
1 |
True |
The table lists the enumeration values for Previous Alarm State.
|
Enumeration value |
Enumeration definition |
|
0 |
Normal |
|
1 |
Alarm |
|
2 |
Acknowledged |
|
3 |
Reset |
|
4 |
Disabled |
|
5 |
Fault |
The table lists the enumeration values for System Alarm ID. For more information, see System Alarm ID Enumerations .
The table lists the enumeration values for System Event ID. For more information, see System Event ID Enumerations .