earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 2.0, 2.1, 3.0, 3.1
02/01/2019

Event View Properties

Use the Event View properties for viewing and editing the properties of the Events pane and Event View.

 
action_zoom_plus_stroke Event View properties
Figura: Event View properties

Tabla: Event View Properties

Component

Description

Show milliseconds

Select True to display time properties including milliseconds.

Number of records shown

Enter the number of rows you want to list in the Events pane or Event view. You can enter any number between 1 and 5999.

Aviso
  • By default, the latest 1000 event records are displayed in the Event View.

  • Regardless of the number of event records in the database, you can display a maximum of 5999 event records at a time in the Event View.

  • You can use the filter to display a different set of event records, maximum 5999 records at a time.

  • Events Pane and Event View Customization
  • Panel de eventos y vista de eventos