earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 3.2, 3.3, 2022
21/06/2023

Events Pane and Event View Customization

You can style certain events to bring out those that are of more interest than other events listed in the Events pane and Event Views. To style a specific event, you first have to create a condition that is associated with the events you want to style. An event can be styled with a unique background color, font, and font color.

For example, you can style all events where an alarm is acknowledged. To separate this event from others you configure, change the background color to dark green and the font color to white. All other events have the default style which is a white background and black font color.

If an event fulfills the condition criteria in more than one of the configured event criteria, it is the event style with highest priority in the Events View Style dialog box that is applied to the event.

Events styling does not apply to WebStation and does not affect the events in WebStation.

Event View standard filter and layout

A standard layout defines the columns that are included in the Alarms pane, Events pane, Alarm View, or Event View, the order in which they are displayed, whether or not the alarms or events are grouped in any way and whether they are displayed in an ascending or descending order. A standard filter defines the conditions that have to be met before the alarms or events are displayed in the pane or a View. The standard layout and filter is saved for the pane or View to which you made the changes. The standard layout and filter is displayed for all users of the the EcoStruxure BMS.

Para obtener más información, consulte Alarm View and Event View Standard Filter and Layout .

  • How Events Work
  • Barra de herramientas del panel eventos y la vista de eventos
  • Panel de eventos y vista de eventos
  • Alarm and Event Detail View
  • Event Styles Dialog Box
  • Event View Properties
  • Alarm View and Event View Standard Filter and Layout
  • Saving an Event View Standard Layout
  • Editing an Event View Standard Filter
  • Resetting the Event View Standard Layout to Factory Default
  • Ajustar el ancho de la columna al contenido
  • Menú contextual del panel de Eventos
  • Menú Acceso directo al panel Eventos - Submenú Ajustes de visualización de Eventos
  • Select Conditions Dialog Box
  • Displaying Milliseconds in Event Views