earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WorkStation
Functionalities: Basic Functionality
Product version: 2024, 7.0
12/3/2024

File Menu

Use the File menu to log off from the system, import and export information, print, and create new objects.

 
action_zoom_plus_stroke File menu
Figure: File menu

Table: File Menu

Command

Description

New

​Click to open the New submenu where you create new objects. For more information, see File Menu – New Submenu .

Open

Click to open an object.

Open in new tab

​Click to open the selected object in a new tab in the work area.

Show in folder

Click to display the object in its location in the System Tree folder structure.

Save

Click to save changes.

Log Off

Click to log off WorkStation. Your session ends and you are sent to the Welcome Window where you can log in again with the same or another user account. For more information, see Building Operation WorkStation Window .

Change Password

Click to open the Change Password dialog box where you change your password. For more information, see Change Password Dialog Box .

Import

Click to open the Open dialog box where you select a previously exported solution that you want to import. After you select a file, the Import dialog box displays.

The Import dialog box provides a summary of information about the imported file and a preview of the names and file structure of the objects to be imported. For more information, see Import Dialog Box .

Export

Click to open the Save As dialog box where you export a solution to a file location on the WorkStation file system.

The Export preview dialog box displays when there are objects in the solution that the EcoStruxure Building Operation software cannot export from the EcoStruxure BMS server. Use this dialog box to view multiple objects that the system can and cannot export from the EcoStruxure BMS server. For more information, see Export Preview Dialog Box .

Print Preview

Click to preview a printout before printing.

Print

​Click to print the selected object.

Print Setup

Click to adjust the print settings.

Properties

Click to open the Properties dialog box where you inspect or change properties for the selected object. For more information, see General Information Properties – Basic Tab .

Shortcut Properties

​Displays the Properties dialog box for the currently selected shortcut.

Exit

Click to quit WorkStation.

  • File Menu – New Submenu
  • Building Operation WorkStation Window
  • Change Password Dialog Box
  • Import Dialog Box
  • General Information Properties – Basic Tab