earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
4
Koncept

Koncept


Produkter: WorkStation, WebStation
Funktionaliteter: Grundläggande funktionalitet
Produktversion: 3.0, 3.1, 3.2, 3.3, 2022
2019-05-13

Forced Values

When you force a value, all input from the system is overridden. For example, a schedule is set to start a fan at 09:00 but you want it to start at 08:00. In this case, you can force the fan to start at 08:00.

You can manually release a forced value at any time or you can automate the release, using a Timed Force utility object to specify the duration or end time of the force. Mer information finns i Timed Force Objects .

When you release a forced value, the value returns to its normal status.

In WorkStation, you can view the unforced value, which is the real value from the system, at any time. Mer information finns i Viewing an Unforced Value .

Indication in WorkStation

A forced value is indicated by orange color in the properties dialog boxes. In in the Watch pane, a forced value is indicated by a pointing hand

 
action_zoom_plus_stroke
.

In the List View and Search View, a forced value is indicated by the text [Forced] in the 'Value' column.

In WorkStation, you can view the unforced value, which is the real value from the system, at any time. Mer information finns i Viewing an Unforced Value .

Indication in WebStation

A forced value is indicated by orange color and a pointing hand in the List view.

Indication in Function Block Graphics Viewer

A forced value is indicated by orange color in Function Block Graphics Viewer. Mer information finns i Forced Value Indication in Function Block Graphics Viewer .

  • WorkStation Overview
  • WebStation Overview
  • Modify Values
  • Changing Value Dialog Box
  • Configure Dialog Box – Configuration Tab
  • Configure Dialog Box – Operation Tab
  • Force and Unforce Buttons
  • Forcing a Value
  • Forcing a Value
  • Timed Force Objects
  • Releasing a Forced Value
  • Releasing a Forced Value
  • Viewing an Unforced Value
  • Searching for Forced Values
  • Add/Remove Columns Dialog Box (List View)
  • Add/Remove Columns Dialog Box (Search)
  • Forced Value Indication in Function Block Graphics Viewer