earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
功能: 基本功能
产品版本: 1.8
2016/10/13

General Information Properties – Basic Tab

Use the Basic tab to configure and view the General Information properties.

 
action_zoom_plus_stroke General Information properties – basic tab
图: General Information properties – basic tab

表格: General Information Properties

Component

Description

Name

​Displays the name of the object.

Description

Type a description that explains what the object is used for.

Type

​Displays the object type that defines the properties of the object.

Foreign address

Displays the address to a non-Building Operation device, for example a BACnet device.

Modified

​Displays the date and time when the object was last modified.

Note 1

Type text that you display in a graphic or use when searching for the object.​

Note 2

​Type text that you display in a graphic or use when searching for the object.

Validation

Select the validation status of the object to keep track of which objects have passed or failed the validation.

Executed by

Indicates the object is executed by a BACnet device. An empty field indicates the object is executed by an Automation Server or Enterprise Server.

  • Object Properties
  • References Tab