earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos WebStation
Funcionalidades: Funcionalidad básica, Gestión de usuarios
Versión del producto: 2.0, 2.1, 3.0, 3.1
02/09/2021

Guest Logon in WebStation

A guest logon is used when you want the user to get immediate access to the EcoStruxure Building Operation software using WebStation.

When using a guest logon for WebStation, the user does not have to provide a user name or password. Anyone who tries to access the system is logged on automatically if the guest log on is used.

The guest logon is created using WorkStation and must be named GUEST and use the password GUEST. The guest logon is valid for the domain it is created on. The guest logon can be added to any user group in the system.

The guest account can be used immediately after you have created it. But if you have logged on to WebStation before you created the guest account, you have to clear cookies in the browser to log on automatically using the guest account.

  • User Account Management Overview
  • Creación de cuentas de usuario y administrador en WebStation
  • User Accounts and User Account Groups