You can change and force values using a graphic or the Properties pane. Using the Watch pane, you can dynamically monitor a value.
When you force a value, you override all input from the system. For example, if a schedule is set to enable a device at 09:00, but you want to enable it at 08:00, you can force the enablement at 08:00.
For more information, see Forced Values .
You can add or change units and prefixes on values using WebStation.
For more information, see Adding or Changing a Unit and Prefix for a Value in WebStation .