You can hide or disable alarms to decrease the number of alarms that are presented in the Alarms pane or Alarm View. This is particularly useful when you have many active alarms at the same time.
Hidden and disabled alarms can be displayed and enabled again at any time.
In the Alarms pane or Alarm View, you can hide alarms to decrease the number of alarms and sort out alarms from the list.
For more information, see Hide and Show Alarms .
In the Alarms pane or Alarm View, you can disable an alarm. For example, you can disable an alarm if you need to do maintenance that you know will trigger the alarm.
For more information, see Disable and Enable Alarms .
In the Alarms pane or Alarm View, you recheck alarms to refresh the information.
For more information, see Rechecking Alarms .