User actions are used to ease the understanding of what triggered the alarms and what to do to solve the cause of the alarm. User action can be mandatory or optional depending on how the system is set up.
You can add a comment to an alarm that can be helpful the next time the same alarm is triggered.
For more information, see Alarm Comments .
A cause note is a predefined note that contains information on what triggered the alarm. This information can be helpful the next time the same alarm is triggered.
For more information, see Cause Notes .
An action note is a predefined note that contains information on what you have done to solve the problem that triggered the alarm.
For more information, see Action Notes .
Checklists are predefined lists with steps you take to correct the cause of the alarm.
For more information, see Checklists .