earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 2.0, 2.1, 3.0, 3.1
18/05/2018

Importing a Backup Set to SmartX Server

You import a backup set from a network storage location to restore a replacement SmartX server, or to replace a lost or damaged backup set.

Afficher plus
action_close

You import a backup set from WorkStation to replace a lost or incomplete backup set, or to add a backup set to a new EcoStruxure BMS server. The EcoStruxure Building Operation software stores a local backup set for an Enterprise Server or SmartX servers under the Local folder in the Backup Sets folder. However, the system handles the storage of backup sets based on the type of EcoStruxure BMS server. For example, a SmartX server stores only one backup set at a time. Therefore, the system overwrites the previous backup file with the latest file. If there is no file present, the EcoStruxure Building Operation software adds the backup set to the Local folder.

In a multi-server system with an Enterprise server and SmartX servers, the Enterprise Server retrieves and stores the latest backup set for each SmartX server in a separate directory in the Backup Sets folder. In addition, the system can store several backup sets for each SmartX server as well as multiple backup sets for the Enterprise Server.

In a multi-server system with an Enterprise Central, the Enterprise Central does not retrieve and store the backup set for each Enterprise Server on the computer that runs the Enterprise Central. When you restore an Enterprise Server from an Enterprise Central, you use the backup sets that are stored on the computers running the Enterprise Servers.

Déclaration

When you back up the Enterprise Servers from an Enterprise Central, the SmartX servers that are attached to the Enterprise Servers are not backed up. To make a backup of Smart X server you start by backing up the Smart X servers using the Enterprise Servers. When that is done, you back up all the Enterprise Servers using the Enterprise Central.

 
action_zoom_plus_stroke Import backup set from WorkStation to a SmartX servers or Enterprise Server
Figure : Import backup set from WorkStation to a SmartX servers or Enterprise Server

Importing is a three-step process: logging onto the EcoStruxure BMS server, importing the file, and then restoring the EcoStruxure BMS server. First, you log onto an EcoStruxure BMS server in WorkStation. You then import the selected backup set from a network storage area. Finally, you restore the EcoStruxure BMS server.

You can only restore an EcoStruxure BMS server using a backup set that was created with the same software version on the same EcoStruxure BMS server (including service pack). To help identify the usable backup sets, the system displays the compatible files in black text and the incompatible files in red text. If you select an incompatible backup set to restore an EcoStruxure BMS server, no backup set displays after importing.

To import a backup set to SmartX server
  1. Log on to the SmartX server to which you want to import a backup set.

  2. In WorkStation, in the System Tree pane, select the SmartX server.

  3. On the Actions menu, click Restore .

  4. In the Restore Options dialog box, click Import Backup Set .

  5. In the Confirm Replace dialog box, click OK .

  6. Select a valid backup set that is stored on a file system and click Open .

  7. Click Close .

You can now restore the SmartX server with the imported backup set.

  • Restoring the EcoStruxure BMS Server
  • Restore Options Dialog Box
  • No Restore Files Display After Backup
  • Backup Set Import from WorkStation