earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos Enterprise Server, Function Block Editor, Graphics Editor, License Administrator, License Server, Script Editor, Software Administrator
Funcionalidades: Funcionalidad básica, Actualizar
Versión del producto: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
18/05/2018

Installation Wizard – License Server Configuration Page

Use the License Server Configuration page to configure the address to the license server.

 
action_zoom_plus_stroke License server configuration page
Figura: License server configuration page

Tabla: License Server Configuration Page

Component

Description

License Server Address

Type the address to the license server where licenses are available for check out. The address must begin with @. To define the port number, if other than the default port range 27000-27009, type the port number in front of the @, Port-number@Address. Use a semicolon to separate addresses.

  • Installation Overview
  • Server Installation Wizard – Configuration Page
  • Installation Wizard – Choose Components Page
  • Installation Wizard – Installation Type Page
  • License Administrator