earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: Enterprise Server, Function Block Editor, Graphics Editor, ​License Administrator, ​License Server, Script Editor, Software Administrator
功能: 基本功能, 升级
产品版本: 2024, 7.0
2024/12/2

Installation Wizard – License Server Configuration Page

Use the License Server Configuration page to configure the address to the license server.

 
action_zoom_plus_stroke License server configuration page
图: License server configuration page

表格: License Server Configuration Page

Component

Description

License Server Address

Type the address to the license server where licenses are available for check out. The address must begin with @. To define the port number, if other than the default port range 27000-27009, type the port number in front of the @, Port-number@Address. Use a semicolon to separate addresses.

  • Installation Overview
  • Server Installation Wizard – Configuration Page
  • Installation Wizard – Choose Components Page
  • Installation Wizard – Installation Type Page
  • License Administrator