Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
You install WorkStation and client tools to create and supervise your EcoStruxure BMS.
Ensure that you have working and available WorkStation, Graphics, Script, WorkPlace Tech Editor, and Menta / Function Block licenses. A working license for each product is required to start and log on. For more information, see Licenses .
It is recommended that you install the latest release of .NET 4.5 version before installing WorkStation and Client Tools.
Install the latest release of .NET version 4.5.
Double-click on the WorkStation installation file to start the installation wizard.
If User Account Control (UAC) is enabled, you must run the installer as administrator. Right-click the installation file and then click Run as administrator .
Click Yes to confirm that you want to run the Workstation installation package.
In the Installation wizard, click Next .
In the License Agreement page, make sure that you agree with the End User License Agreement (EULA) and then click I Agree .
In the Installation Folder page, browse to the folder where you want to install WorkStation and client tools and then click Next .
When upgrading to a later version, the installation path is changed to the default installation folder for that version. The default installation folder is always located on the C: drive
The complete installation path can have maximum 115 characters.
EcoStruxure Building Operation products are installed in the same folder that you selected for the first product you installed.
If you are installing WorkStation and client tools on a 64-bit operating system and you specify a location under \Program Files\ , WorkPlace Tech Editor and its components are installed in the folder \Program Files (x86)\ .
In the Choose Components page, select the components that you want to install and then click Next .
Before selecting the WorkPlace Tech Editor component, be sure the appropriate versions of Microsoft Visio and .NET 3.5 SP1 are installed.
For more information, see EcoStruxure Building Operation Software Requirements .
In the WorkStation Shortcut Selection page, select the shortcuts you want to be created and then click Next .
In the License Server Address box, type @ and then type the address to the license server.
If the License Server uses a port other than the default port range 27000-27009, type the port number in front of @. For example, 567@localhost.
Use a semicolon to separate addresses to different License Servers.
Click Install .
Click Next .
Click Finish .
Click Show details to follow the progress of the installation.