earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Trends
Product version: 2023, 2024
12/17/2022

Interval Trend Log Properties – Basic Tab

Use the Basic tab to configure the Interval trend log.

 
action_zoom_plus_stroke Interval trend log properties - Basic tab
Figure: Interval trend log properties - Basic tab

Table: Interval Trend Log Properties - Basic Tab

Property

Description

Status

Displays the status of the trend log.

Enabled

Displays True if the trend log is enabled.

Logged variable

Enter the variable you want to log.

Delta

Select the minimum value change that triggers a new record.

For more information, see Interval Trend Log Delta .

Activation variable

Enter the variable that makes the trend log start recording values when the variable is True .

For more information, see Trend Log Activation .

Activation time

Specify the time when the trend log is to start recording values.

For more information, see Trend Log Activation .

Interval

Type how often to log the variable. The interval defines the time between two log records.

Log size

Select the number of records to store before old records are overwritten, including internal records generated by the trend log.

For more information, see Log Record Storage .

Clear when enabled

Select True to clear the trend log when it is enabled.

  • Trend Log Types
  • Interval Trend Logs
  • Configure Dialog Box – Configuration Tab
  • Interval Trend Log Delta
  • Trend Log Activation
  • Configure Dialog Box – Operation Tab
  • Log Record Storage
  • Trend Log Does Not Start Record Due to the Start Condition
  • Missing Trend Log Records
  • General Information Properties – Basic Tab
  • References Tab