earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AO-8, AO-V-8, Automation Server, DI-16, DO-FA-12, DO-FC-8, AS-P, PS-24V, RTD-DI-16, UI-16, UI-8/AO-4, UI-8/AO-4 v2, UI-8/AO-V-4, UI-8/AO-V-4 v2, UI-8/DO-FC-4, UI-8/DO-FC-4 v2
Functionalities: Central IO , Hardware
Product version: 2.0, 2.1, 3.0, 3.1
5/22/2019

I/O Bus Restrictions

The I/O bus imposes restrictions on the number of devices that can be connected to the bus and what type of devices that are allowed on certain positions.

The following restrictions apply to the I/O bus:

  • Position 1 reserved for a power supply

  • Position 2 reserved for a SmartX AS-P server or Automation Server

  • Maximum one SmartX AS-P server or Automation Server per I/O bus

  • Maximum 32 devices per I/O bus

Note:

Even when connected by an S-cable, no more than 32 devices are allowed on the I/O bus.

  • Terminal Bases
  • I/O Bus
  • I/O Bus Parts
  • Power Budget
  • Configuring an I/O Module