earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: AO-8, AO-V-8, DI-16, DO-FA-12, DO-FC-8, AS-P, PS-24V, RTD-DI-16, UI-16, UI-8/AO-4, UI-8/AO-4 v2, UI-8/AO-V-4, UI-8/AO-V-4 v2, UI-8/DO-FC-4, UI-8/DO-FC-4 v2
Funktionaliteter: I/O-kommunikation, Maskinvara
Produktversion: 3.3, 2022, 2023, 2024, 7.0
2025-07-04

I/O Bus Restrictions

The I/O bus imposes restrictions on the number of devices that can be connected to the bus and what type of devices that are allowed on certain positions.

The following restrictions apply to the I/O bus:

  • Position 1 reserved for a power supply

  • Position 2 reserved for a AS-P server

  • Maximum one AS-P server per I/O bus

  • Maximum 32 devices per I/O bus

Obs!

Even when connected by an S-cable, no more than 32 devices are allowed on the I/O bus.

  • Terminal Bases
  • I/O Bus
  • I/O Bus Parts
  • Power Budget
  • Configuring a Central IO Module