earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AO-8, AO-V-8, AS-L, DI-16, DO-FA-12, DO-FC-8, AS-P, PS-24V, RTD-DI-16, UI-16, UI-8/AO-4, UI-8/AO-V-4, UI-8/DO-FC-4
功能: I/O 通信, 硬件
产品版本: 2.0, 2.1, 3.0, 3.1
2019/5/22

I/O Bus Restrictions

The I/O bus imposes restrictions on the number of devices that can be connected to the bus and what type of devices that are allowed on certain positions.

The following restrictions apply to the I/O bus:

  • Position 1 reserved for a power supply

  • Position 2 reserved for a SmartX AS-P server or Automation Server

  • Maximum one SmartX AS-P server or Automation Server per I/O bus

  • Maximum 32 devices per I/O bus

注释:

Even when connected by an S-cable, no more than 32 devices are allowed on the I/O bus.

  • Terminal Bases
  • I/O Bus
  • I/O Bus Parts
  • Power Budget
  • Configuring an I/O Module