Configuration Menus are a group of pre-engineered objects and values that make device commissioning faster and easier. Configuration Menus are exported and downloaded from image files. Download a Configuration Menu to a BACnet/IP controller to commission the controller.
You download an Application Image that contains a Configuration Menu to a BACnet/IP controller to configure a device. Use this workflow to implement the Configuration Menu using the Commission mobile application. Related information can be found in the section after the flowchart.
For more information, see Configure Controllers with the Configuration Menu Workflow .
You download the Configuration Menu to the BACnet/IP controller to configure the device.
For more information, see Downloading a Configuration Menu to a BACnet/IP Controller .
After downloading the configuration menu to the controller, you view and modify the device properties from the configuration menu to complete device commissioning.
For more information, see Modifying Device Properties from the Configuration Menu .