earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: Enterprise Central, Enterprise Server, Project Configuration Tool
功能: 基本功能
产品版本: 2024, 7.0
2025/10/30

Properties Conditions Search

​You can search for object properties and exclude irrelevant search results by defining which property types to search for and by setting up conditions for which properties you want to include in the search.

If you have defined the property type you want to search for, you get suggestions to help you find the localized name of the property.

 
action_zoom_plus_stroke The Select Conditions dialog box when no object type is selected in the Include types dialog box.
图: The Select Conditions dialog box when no object type is selected in the Include types dialog box.

​If you choose to include one or more object types in the search, you can select a condition from the common properties for these object types. If no object type is included in the search, you can select conditions from the general properties for all object types.

If you include only one object in the search you can choose between all the properties for that object type. For example, if you choose Alarm you can select from all alarm properties in the Selection dialog box.

​For example, to search for disabled alarms, you select alarm object type and then select alarm state in the property list.

 
action_zoom_plus_stroke The properties available in the Select Conditions dialog box when alarm is selected in the Include types dialog box.
图: The properties available in the Select Conditions dialog box when alarm is selected in the Include types dialog box.

The conditions format varies depending on property type.

When a property is included in the search result, you can navigate to the object it belongs to from the Search View.

If your search result includes a property you want to monitor, you can drag the property from the Search View to the Watch pane.

Combining condition groups

You can combine condition groups to better suit your search. The different conditions groups can be combined in any way using "and" and "or".

For example, we want to find all analog values that contain "Setpoint" or "setpoint" in their object names or descriptions. The objects we want to find have a values over 20 or have been modified after 2013-02-25 00:00:00.

A search on these criteria looks like this:

 
action_zoom_plus_stroke You can combine different search criteria in conditions groups to further refine your search.
图: You can combine different search criteria in conditions groups to further refine your search.
注释:

Strings in the Select Conditions dialog box are case sensitive, that is they differ between upper and lower case. A description condition for the text string "temperature" is not the same as "Temperature".

  • Search
  • Search Overview
  • Searching for Objects or Properties