earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: WebHelp
Funktionaliteter: Grundläggande funktionalitet
Produktversion: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
2021-08-27

Languages

In WebHelp, the default language is English but you can also access information that has been translated into other languages.

WebHelp displays its content in the same language that your web browser uses, provided that the WebHelp content has been translated to your language. When selecting a language in the WebHelp Language box, your browser settings are overridden. The Language box setting is stored into the URL address.

Obs!
  • When you bookmark or copy a WebHelp address to distribute it, the URL contains information about which language to display, if a language has been selected in the Language box.

If you are logged on to WebHelp when you select the language, your language preference is stored to your user profile. This means that your defined language is displayed when you revisit WebHelp.

The Schneider Electric sales companies, subsidiaries, or partners of each country decide which information is translated.

  • Features
  • WebHelp Overview
  • WebHelp Home Page