earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: License Administrator, License Server
Funktionaliteter: Licenshantering
Produktversion: 2024
2024-12-03

EcoStruxure Building Operation Software License Backup and Restore

Backup the EcoStruxure Building Operation software license files on a regular basis. To back up the license files, copy all files in the folder to an external resource. Backups are useful if the hardware or the operating system malfunctions.

Backed up licenses can only be restored on the same License Server that the files were backed up from. If you plan to move the licenses to another License Server, you first must return the licenses to the License Activation Server and then activate them on the new License Server. Mer information finns i EcoStruxure Building Operation Software License Return .

The license files are located in: \ProgramData\FLEXnet in Windows.

The restored licenses files may on rare occasions be considered damaged by the License Server. If so, they must be repaired. Mer information finns i EcoStruxure Building Operation Software License Repair .

  • EcoStruxure Building Operation Software License Maintenance
  • EcoStruxure Building Operation Software License Repair
  • Backing Up EcoStruxure Building Operation Software Licenses
  • Restoring EcoStruxure Building Operation Software Licenses
  • EcoStruxure Building Operation Software Requirements