earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: ​License Administrator, ​License Server
功能: 许可证管理
产品版本: 1.8, 1.9
2015/5/28

License Management

A Building Operation license system consists of, for example, a License Server, WorkStation with client tools, and the Enterprise Server. The number of each component varies depending on the system size and architecture.

In this example, the License Server and Enterprise Server are located on the same computer. Several WorkStations check out licenses from the License Server through the local area network. Network licenses are activated on the License Server by the License Activation Server that is controlled by Schneider Electric.

 
action_zoom_plus_stroke WorkStation system with License Server and Enterprise Server on same computer and WorkStation in separate computers, one computer with client tool.
图: WorkStation system with License Server and Enterprise Server on same computer and WorkStation in separate computers, one computer with client tool.

License System Installation and Configuration

Schneider Electric recommends that you install the license server framework before other Building Operation software or SmartStruxure server devices. The license server installation is included in the License Administrator license package. During the installation of WorkStation or Enterprise Server, the installation software asks for the address to the license server.

有关更多信息,请参阅 Installation Example .

Network License Management

When you activate a license, the license is transferred from the License Activation Server to your License Server. When activating a license, details about the transaction and registration details are stored with the license on the License Server.

有关更多信息,请参阅 Network License Management .

Local License Management

A local license is activated from a license file with the extension .asr. Local licenses must be activated to a dedicated WorkStation or Enterprise Server computer. The local license cannot be distributed and shared between different computers as the network license can.

有关更多信息,请参阅 Local License Management .

  • Licensing Overview
  • Network License Management
  • Local License Management
  • Installation Example