earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: License Administrator, License Server
Funcionalidades: Gestão de licenças
Versão do produto: 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
29-01-2020

License Server Address View

Use the License Server Address view to specify the address to the License Server.

 
action_zoom_plus_stroke License Server address view
Imagem: License Server address view

Tabela: License Server Address View

Component

Description

License server address

Type the address to the License Server where licenses are available for check out. The address must begin with @. To define a port number other than the default port range 27000-27009, type the port number in front of the @, Port-number@Address. Use a semicolon to separate addresses.

  • License Administrator
  • Licenses View Icons
  • Diagnostics View
  • Unable to Activate EcoStruxure Building Operation Software Licenses