earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Conceito

Conceito


Produtos: AS-B, Enterprise Central, Enterprise Server, License Administrator, License Server, AS-P
Funcionalidades: Gestão de licenças
Versão do produto: 3.3, 2022
11-11-2024

EcoStruxure Building Operation Software Licensing Installation and Location

It is recommended that License Administrator and License Server run on the same computer as Enterprise Server or Enterprise Central that use the licenses.

Schneider Electric recommends that you install the license server framework before installing other EcoStruxure Building Operation software applications and automation servers. License Server installation is included in the License Administrator license package. During the installation of WorkStation, Enterprise Server, or Enterprise Central, the installation software asks for the address to License Server.

In this example, the License Server and Enterprise Server are located on the same computer. Several WorkStations check out licenses from the License Server through the local area network. Licenses are activated on the License Server by the License Activation Server that is controlled by Schneider Electric.

 
action_zoom_plus_stroke WorkStation system with License Server and Enterprise Server on same computer and WorkStation in separate computers, one computer with client tool.
Imagem: WorkStation system with License Server and Enterprise Server on same computer and WorkStation in separate computers, one computer with client tool.

When you activate a license, the license is transferred from the License Activation Server to your License Server. When activating a license, details about the transaction and registration details are stored with the license on the License Server.

License Server Installation and Location

License Identification Overview

Use one separate License Server for every Enterprise Central and Enterprise Server to get an overview of your licenses. If two or more Enterprise Servers or Enterprise Centrals gets their licenses from the same License Server, you cannot identify which Enterprise Server or Enterprise Central got the license.

If you need to repair or move an EcoStruxure Building Operation software license, the request must come from the License Server that was used to activate the license.

If you try to install Enterprise Server or Enterprise Central on a computer without a License Administrator, you get the system alarm "Invalid license server configuration". 

License Server Location

Install the License Server and Enterprise Server or Enterprise Central on the same computer to avoid license problems caused by network problems. Use the address @localhost so the Enterprise Server cannot connect to the License server through the network.

License Server Internet access

Ensure that the License Server has access to the Internet and to the local area network. Internet access is necessary when performing tasks that require communication with the License Activation Server, such as activating or returning licenses on your License Server. Instant access to the local area network ensures that licensed WorkStations, client tools, Enterprise Servers, and Enterprise Centrals can check out and check in licenses.

Nota

For security reasons, Internet access can be disconnected when communication with the License Activation Server is not needed.

License Administrator Installation and Location

Install License Administrator on the same computer as the Enterprise Server or Enterprise Central. This makes your system less vulnerable to network failure.

  • EcoStruxure Building Operation Software Licensing Overview
  • EcoStruxure Building Operation Software Licensing Workflow
  • Licenses Activation Server
  • License Server
  • License Administrator