earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos License Administrator, License Server
Funcionalidades: Gestión de licencias
Versión del producto: 3.0, 3.1
30/11/2019

Licensing Overview

arrow1_rotationLicensing Model arrow1_rotationLicense System arrow1_rotationLicense Management arrow1_rotationService and Maintenance arrow1_rotationLicense Information arrow1_rotationDevice Administrator Licenses

The EcoStruxure Building Operation software is available for all to download and install. However, you need valid licenses to use the software. The number of users of the software is limited to the number of licenses owned by the customer.

Licensing Model

EcoStruxure BMS uses a license model that allows scalable pricing. An EcoStruxure BMS can be tailored with the features and size that is required by that solution. When setting up a new EcoStruxure BMS, consider the size, the extra features required, and the number of licenses to accommodate the size and features. The license policy lets you make an initial investment that corresponds to the required capacity and functionality at the beginning of the project and then allows for further investment in the future to expand the capacity or functionality.

Para obtener más información, consulte Licensing Model .

License System

​When setting up a new EcoStruxure BMS, you need to consider the size of the system, its structure, and the number of licenses to order and distribute.

Para obtener más información, consulte License System .

License Management

The EcoStruxure Building Operation license system consists of, for example, a License Server, WorkStation with client tools, and the Enterprise Server. The number of each component varies depending on the system size and architecture.

Para obtener más información, consulte License Management .

Service and Maintenance

The EcoStruxure Building Operation license policy is strictly controlled and is sensitive to any changes on the License Server, both hardware and software.

Para obtener más información, consulte Service and Maintenance .

License Information

The License Information in the Control Panel gives you an overview of the licenses in your EcoStruxure BMS.

Para obtener más información, consulte License Information .

Device Administrator Licenses

Device Administrator is used to manage licenses on SmartX server.

Para obtener más información, consulte Device Administrator Licenses .

  • Licensing, Installation, and Localization Overview
  • License System
  • License Management
  • Service and Maintenance
  • License Information
  • Device Administrator Licenses