earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Server, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 1.8
10/13/2016

Local Backup and Restore of SmartStruxure Servers

In WorkStation, you can log on to a SmartStruxure server directly to perform manual backup and restore tasks.

Local Backup and Restore of a Standalone SmartStruxure Server Devices

In WorkStation, you can log on to SmartStruxure server device to perform a manual backup of the SmartStruxure server device data. If you have multiple standalone SmartStruxure server devices, the Backup and Restore processes on one SmartStruxure server device remain self-contained and, therefore, separate from any another SmartStruxure server device on the network.

 
action_zoom_plus_stroke Backup and Restore for multiple standalone SmartStruxure Server Devices
Figure: Backup and Restore for multiple standalone SmartStruxure Server Devices

The system only stores one backup file at a time on the SmartStruxure server devices. If you import a backup set, the system overwrites the locally stored file with the imported file. Therefore, you will only see one backup file in the Restore Options dialog box when you log on to a SmartStruxure server device.

Local Backup and Restore of an Enterprise Server

In WorkStation, you can log on to an Enterprise Server to perform a manual backup of the Enterprise Server data. If you have multiple Enterprise Servers, the Backup and Restore processes on one Enterprise Server remain self-contained and, therefore, separate from any another Enterprise Server on the network.

 
action_zoom_plus_stroke Backup and Restore for multiple Enterprise Servers
Figure: Backup and Restore for multiple Enterprise Servers
  • Manual Backups
  • Backup Sets
  • Backup Set Properties – Basic Tab