earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 1.9
25/04/2017

Local Backup and Restore of SmartStruxure Servers

In WorkStation, you can log on to a SmartStruxure server directly to perform manual backup and restore tasks.

Local Backup and Restore of a Standalone SmartStruxure Server Device

In WorkStation, you can log on to a SmartStruxure server device to perform a manual backup of the SmartStruxure server device data.

If you have multiple standalone SmartStruxure server devices, the Backup and Restore processes on one SmartStruxure server device remain self-contained and, therefore, separate from any another SmartStruxure server device on the network.

In a stand-alone system only one backup set is stored on the SmartStruxure server device. If you import a backup set, the system overwrites the locally stored file with the imported file. Therefore, you only see one backup file in the Restore Options dialog box when you log on to a SmartStruxure server device.

Local Backup and Restore of an Enterprise Server

In WorkStation, you can log on to an Enterprise Server to perform a manual backup of the Enterprise Server data. If you have multiple Enterprise Servers, the Backup and Restore processes on one Enterprise Server remain self-contained and, therefore, separate from any another Enterprise Server on the network.

  • Manual Backups
  • Backup Sets
  • Backup Set Properties – Basic Tab