earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2024, 7.0
2024/12/2

Local Backup and Restore of EcoStruxure BMS Servers

In WorkStation, you can log on to an EcoStruxure BMS server directly to perform manual backup and restore tasks.

Local Backup and Restore of a Standalone Automation Server

In WorkStation, you can log on to an automation server to perform a manual backup of the automation server data.

If you have multiple standalone automation servers, the Backup and Restore processes on one automation server remain self-contained and, therefore, separate from any another automation server on the network.

In a stand-alone system only one backup set is stored on the automation server. If you import a backup set, the system overwrites the locally stored file with the imported file. Therefore, you only see one backup file in the Restore Options dialog box when you log on to an automation server.

Local Backup and Restore of an Enterprise Server

In WorkStation, you can log on to an Enterprise Server to perform a manual backup of the Enterprise Server data. If you have multiple Enterprise Servers, the Backup and Restore processes on one Enterprise Server remain self-contained and, therefore, separate from any another Enterprise Server on the network.

Local Backup and Restore of an Enterprise Central

In WorkStation, you can log on to an Enterprise Central to perform a manual backup of the Enterprise Central data. The Backup and Restore processes on Enterprise Central are self-contained.

  • Manual Backups
  • Backup Sets
  • Backup Set Properties – Basic Tab