earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: License Administrator, License Server
Funktionaliteter: Licenshantering
Produktversion: 3.2, 3.3
2020-07-15

EcoStruxure Building Operation Demo License Management

Demo licenses for EcoStruxure Building Operation software are local, bound to the computer, and cannot be shared.

The license file used to activate demo licenses can only be used once per computer and is time-limited. The demo license is installed on License Server from a license file with the extension .asr. Demo licenses must be activated on the same computer that runs WorkStation, Enterprise Server or Enterprise Central.

 
action_zoom_plus_stroke A local license is activated on the computer that will use it and cannot be shared with other computers.
Figur: A local license is activated on the computer that will use it and cannot be shared with other computers.

EcoStruxure Building Operation Demo Licensing Workflow

Use this workflow to add demo licenses for EcoStruxure Building Operation software running on Windows.

Mer information finns i EcoStruxure Building Operation Demo Licensing Workflow .

EcoStruxure Building Operation License Activation

Use the License Administrator on the WorkStation or Enterprise Server depending of where you want to activate the demo license.

 
action_zoom_plus_stroke Activation of demo license on a WorkStation with a demo license file
Figur: Activation of demo license on a WorkStation with a demo license file

Demo License Removal

To remove a demo license, use the License Administrator on the WorkStation or Enterprise Server where the demo license is activated.

Mer information finns i Removing an EcoStruxure Building Operation Software Demo License .

  • EcoStruxure Building Operation Demo Licensing Workflow
  • Activating an EcoStruxure Building Operation Demo License