earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Gestión de usuarios
Versión del producto: 2.0, 2.1, 3.0, 3.1
18/05/2018

Log On Methods

The EcoStruxure Building Operation software provides two methods to log on to the system: as a Windows user or as an EcoStruxure Building Operation user.

Log On as a Windows User

If you are logged on with a Windows user account that is mapped to the Windows Active Directory user account group that you belong to, you can select an EcoStruxure BMS server and log on in a single sign-on. Para obtener más información, consulte Inicio de sesión en WorkStation usando su cuenta de usuario de Windows .

You can also log on using another Windows account that is mapped. Para obtener más información, consulte Inicio de sesión en WorkStation como otro usuario de Windows .

Log On as an EcoStruxure Building Operation User

When logging on as an EcoStruxure Building Operation user, you authenticate yourself with an EcoStruxure Building Operation account user name and password. Para obtener más información, consulte Inicio de sesión en WorkStation como usuario de EcoStruxure Building Operation .

You also select which EcoStruxure Building Operation domain and EcoStruxure BMS server that you want to access. Para obtener más información, consulte User Accounts and User Account Groups .

With an EcoStruxure Building Operation user account, you can also connect directly to the local domain of an EcoStruxure BMS server. Para obtener más información, consulte Administration Accounts in EcoStruxure BMS Server Local Domain .

Password Administration

As a WorkStation administrator, you can change users’ passwords, force users to change their passwords at next logon, or enable and disable the possibility for users to change their passwords.

Para obtener más información, consulte Password Administration .

  • Inicio de sesión en WorkStation usando su cuenta de usuario de Windows
  • Inicio de sesión en WorkStation como otro usuario de Windows
  • Inicio de sesión en WorkStation como usuario de EcoStruxure Building Operation
  • Windows Active Directory User Groups
  • User Accounts and User Account Groups
  • Administration Accounts in EcoStruxure BMS Server Local Domain
  • Password Administration
  • User Account Management Overview
  • Resolving Enterprise Server or Enterprise Central Port Conflicts