earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Produits : AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Gestion des utilisateurs
Version produit : 3.2, 3.3, 2022
15/10/2020

Log On Methods

The EcoStruxure Building Operation software provides two methods to log on to the system: as a Windows user or as an EcoStruxure Building Operation user.

Log On as a Windows User

If you are logged on with a Windows user account that is mapped to the Windows Active Directory user account group that you belong to, you can select an EcoStruxure BMS server and log on in a single sign-on. Pour plus d'informations, voir Connexion à WorkStation à l'aide de vos identifiants Windows .

You can also log on using another Windows account that is mapped. Pour plus d'informations, voir Connexion à WorkStation sous un autre nom utilisateur Windows .

Log On as an EcoStruxure Building Operation User

When logging on as an EcoStruxure Building Operation user, you authenticate yourself with an EcoStruxure Building Operation account user name and password. Pour plus d'informations, voir Connexion à WorkStation en tant qu'utilisateur EcoStruxure Building Operation .

You also select which EcoStruxure Building Operation domain and EcoStruxure BMS server that you want to access. Pour plus d'informations, voir User Accounts and User Account Groups .

With an EcoStruxure Building Operation user account, you can also connect directly to the local domain of an EcoStruxure BMS server. Pour plus d'informations, voir Administration Accounts in EcoStruxure BMS Server Local Domain .

Password Administration

As a WorkStation administrator, you can change users’ passwords, force users to change their passwords at next logon, or enable and disable the possibility for users to change their passwords.

Pour plus d'informations, voir Password Administration .

  • Connexion à WorkStation à l'aide de vos identifiants Windows
  • Connexion à WorkStation sous un autre nom utilisateur Windows
  • Connexion à WorkStation en tant qu'utilisateur EcoStruxure Building Operation
  • Windows Active Directory User Groups
  • User Accounts and User Account Groups
  • Administration Accounts in EcoStruxure BMS Server Local Domain
  • Password Administration
  • User Account Management Overview
  • Resolving Enterprise Server or Enterprise Central Port Conflicts