earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Функции: Тренды
Версия продукта: 2024, 7.0
02.12.2024

Log Record Storage

​All trend logs use circular storing. How many records a trend log can store before overwriting old ones depends on the trend log configuration.

For example, a trend log is configured to store 10 records. The logging starts and the first record x1 is stored. After 10 records the trend log is full. The next record x11 overwrites the oldest record which in our case is x1. The next logging x12 overwrites the oldest record x2, and so on.

Additional internal records can be generated by the log itself. These records may not be visible. Internal records are a part of the log usage.

If you try to configure a trend log to store a larger number of log records than the EcoStruxure BMS server can manage, the trend log is not created.

 
action_zoom_plus_stroke Circular storing, schematic
Рисунок: Circular storing, schematic
  • Trend Log Functions
  • Trends Overview
  • Interval Trend Logs
  • Meter Function
  • Change of Value Trend Logs
  • Variable Triggered Trend Logs
  • Manual Trend Logs
  • Editing the Log Size for a Trend Log