You log on to WorkStation or WebStation to securely access the EcoStruxure Building Operation functions.
You log on to WorkStation with your current Windows credentials, as another Windows user, or as an EcoStruxure Building Operation user. Your system administrator decides which type of user you log on as.
To log on to WorkStation using an EcoStruxure Building Operation account, you need to know the following account information:
User name
Password
Domain
EcoStruxure BMS server
To log on to WorkStation using a Windows account, you need to know the EcoStruxure BMS server.
The account information for both the EcoStruxure Building Operation account and the Windows account is provided by the system administrator.
Important:
Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation.
For more information, see Licenses
.
Remember me on this computer
For a faster log on in Workstation, use the Remember me feature to automatically fill in your user name, password, domain and server. Both Building Operation users and Windows users can use the Remember me feature.
Add a display name of the server address
When you log on to a new server, its IP address is added to the server list. You can add a display name of the server address to make it easier to find your server in the list.
Log on to WebStation
To log on to WebStation, you need to know the following account information:
User name
Password
Domain
EcoStruxure BMS server
The account information for your account is provided by the system administrator.