Productos WebStation
Funcionalidades: Funcionalidad básica
Versión del producto: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
03/07/2019
Haga clic para ver la versión actualizada que aún no se ha traducido

Inicio de sesión en WebStation

Puede iniciar sesión en WebStation para acceder a la base de datos de EcoStruxure Building Operation.

Mostrar más
action_close

You log on to WorkStation or WebStation to securely access the EcoStruxure Building Operation functions.

Log on to WorkStation

You log on to WorkStation with your current Windows credentials, as another Windows user, or as an EcoStruxure Building Operation user. Your system administrator decides which type of user you log on as. ​

To log on to WorkStation using an EcoStruxure Building Operation account, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

To log on to WorkStation using a Windows account, you need to know the EcoStruxure BMS server.

The account information for both the EcoStruxure Building Operation account and the Windows account is provided by the system administrator.

Aviso

​​Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation. Para obtener más información, consulte EcoStruxure Building Operation Software Licensing Installation and Location .

Remember me on this computer

For a faster log on in Workstation, use the Remember me feature to automatically fill in your user name, password, domain and server. Both Building Operation users and Windows users can use the Remember me feature.

Add a display name of the server address

When you log on to a new server, its IP address is added to the server list. You can add a display name of the server address to make it easier to find your server in the list.

Log on to WebStation

To log on to WebStation, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

The account information for your account is provided by the system administrator.

Para iniciar sesión en WebStation
  1. En la ventana EcoStruxure Building Operation WebStation, en el cuadro Nombre de usuario , introduzca su nombre de usuario.

  2. En el cuadro Contraseña , introduzca su contraseña.

  3. En el cuadro Dominio , introduzca un nombre de dominio.

  4. Haga clic en Inicio de sesión .

  • Log on to WorkStation or WebStation
  • Ventana de Building Operation WebStation
  • Cierre de sesión en WebStation
  • Cómo cambiar la contraseña