earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
5
User Interface

User Interface


Products: WebReports
Functionalities: Reports
Product version: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
12/16/2021

Manage Images Page

Use the Manage Images page to preview and upload images that can be used in your reports. You can also use the page to delete images from the Image Library. For more information, see WebReports Main Page .

 
action_zoom_plus_stroke Manage Images page
Figure: Manage Images page

Table: Manage Images Page

Component

Description

Image file

Enter the image to be used in your reports.

Image tag

Select a tag that identifies the image in the database. Do not select Factory or Product .

Image name

Type a name for the image. Do not type default .

Save

Click to save the image to the Image Library.

Left image

Select the image to be positioned on the upper left side of your reports.

Right image

Select the image to be positioned on the upper right side of your reports.

Tag/Name

Select the image that you want to delete.

Delete

Click to delete the image from the Image Library.

Preview

Click to view the image before you delete the image.

  • Report Images