Funkcje: Trendy
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Manage Replacement of Meter Dialog Box

Use the Manage replacement of meter dialog box to configure the meter setting when a new meter is installed or replaced.

Uwaga
  • The Manage replacement of meter dialog box only applies to meter trend log.

 
action_zoom_plus_stroke Manage replacement of meter dialog box
Rysunek: Manage replacement of meter dialog box

Tabela: Manage Replacement of Meter Dialog Box

Component

Description

Component

Description

End time

Type the end time of the old meter, preferably the time when the meter is replaced.

End value

Type the value the old meter has when it is replaced.

Unit

Displays the unit of the meter trend log.

Start time

Type the time when the new meter is installed.

Start value

Type the current value of the new meter when it was installed.

Meter constant

Type the constant of the new meter. If the meter counts in kilo (10 3 ) type 1000.

Min value

Type the first value of the new meter after roll-over.

Max value

Type the last value of the new meter before roll-over.

  • Meter Function
  • Meter Trend Log Calculation Fails