earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebReports
Functionalities: Reports
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
12/16/2021

Manage Report Packs Page

Use the Manage Report Packs page to upload and download report packs. You also use the Manage Report Packs page to synchronize new reports that you created in MS Report Builder with the Reports Server. For more information, see WebReports Main Page .

 
action_zoom_plus_stroke Manage Report Packs page
Figure: Manage Report Packs page

Table: Manage Report Packs Page

Component

Description

Reports Tree

Click a report in the Reports Tree to add the report to the report pack. Click a folder to add the contents of the folder to the report pack.

Selected Reports

Displays the reports to be included in the report pack.

 
action_zoom_plus_stroke

Click to remove a report from the Selected Reports box.

 
action_zoom_plus_stroke

Click to remove all of the reports from the Selected Reports box.

Download

Click to download the report pack to a media device. For more information, see Downloading a Report Pack .

Upload Report Pack

Enter the report pack that you want to upload.

Upload

Click to upload the report pack to the Reports Server. For more information, see Uploading a Report Pack .

Exclude Object References

Select to exclude references to extended trend logs, EcoStruxure BMS servers and users. For more information, see Report Packs .

Synchronize

Click to synchronize reports in MS Reporting Services with the Reports Server. Use this feature only if you have created new reports using MS Report Builder.

  • Report Packs
  • Downloading a Report Pack
  • Uploading a Report Pack