earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concetto

Concetto


Prodotti: Enterprise Server, Project Configuration Server, Project Configuration Tool
Funzionalità: Funzionalità di base
Versione del prodotto: 1.8
01/09/2020

Manual and Scheduled Archiving

You can archive data as needed using manual methods or at predefined intervals using a schedule.

Tabella: Comparison of Archiving Methods

Method

Benefits

Manual

Performed on an as-needed basis, for example, prior to upgrading an Enterprise Server. When a Manual Archive is created, the temporary archive data is not deleted. Manual archive creates an incremental archive of everything since the last archiving, manual or scheduled.

Scheduled

Automatically generated by the system at regularly scheduled intervals. When a Scheduled Archive completes, the temporary archive data is deleted.

Scheduled archiving is an automated way of preserving historical data. For convenience, the system provides a default digital schedule, which is bound to the Archive Manager. You can modify, but not delete, this Archive schedule. Per maggior informazioni, consulta Archiving Overview .

  • Archiving Overview
  • Manually Creating an Archive
  • Creating a Scheduled Archive
  • Archive Settings Manager Dialog Box
  • Actions Menu – Actions Submenu