Manual Backup is a non-automated process of copying and storing data on a selected EcoStruxure BMS server. You can use this option to create backups on an as-needed basis. You can also manually restore the data at any time.
You log on to one of the following EcoStruxure BMS servers to initiate a manual backup:
SmartX server or Enterprise Server to perform a local backup. 有关更多信息,请参阅 Local Backup and Restore of EcoStruxure BMS Servers .
Enterprise Server to perform a remote backup of any SmartX servers that are created under the Enterprise Server. 有关更多信息,请参阅 Remote Backup and Restore of SmartX Servers .
Enterprise Central to perform a remote backup of any Enterprise Servers that are created under the Enterprise Central. 有关更多信息,请参阅 Local Backup and Restore of EcoStruxure BMS Servers .
For manual backups, the system initially names the backup set by combining the EcoStruxure BMS server name with the localized date and time of the machine running WorkStation. For scheduled backups, however, the system combines the EcoStruxure BMS server name with the UTC time in the backup set name rather than the local time.
The system also retains the UTC time of manually generated backups. To view the UTC time rather than the localized time for a manual backup set, select the Backup date property from the column selector of the Backup Sets List view. 有关更多信息,请参阅 列 .
If you log on to the Enterprise Server in WorkStation to create a backup of the SmartX server, the system automatically checks for identical backup set names. If a name is found in the AS Archives folder, the system warns of a potential duplication by highlighting the Backup set name prefix box or the Backup set name suffix box in solid red. If you do not change the prefix or suffix, the system displays a red box around the backup set in the Backup set name column to indicate that there is an existing name. If you still do not change the name, the system automatically appends an extended time stamp to prevent the accidental overwriting. 有关更多信息,请参阅 Duplicate Backup Set Names in Multi-server Systems .
In WorkStation, you can log on to an EcoStruxure BMS server directly to perform manual backup and restore tasks.
有关更多信息,请参阅 Local Backup and Restore of EcoStruxure BMS Servers .
When you log on to an Enterprise Server, you can perform remote backups of any SmartX server in the system. Whenever a backup occurs on the SmartX server, the system overwrites the locally stored file on the SmartX server with the new backup file. The Enterprise Server then retrieves and stores this backup file in a separate directory on the computer that runs the Enterprise Server.
有关更多信息,请参阅 Remote Backup and Restore of SmartX Servers .