earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Trends
Product version: 2023, 2024
12/17/2022

Manual Trend Logs

​The manual trend log records data that you manually enter. The manual trend log does not log a variable. Use this type of trend log when values from offline devices have to be manually registered to the trend log. For example, if you want to create a trend log that monitors an electricity meter that cannot be connected to the EcoStruxure BMS.

The default size of a manual trend log is 100 records.

 
action_zoom_plus_stroke Manual trend log schematic.
Figure: Manual trend log schematic.
Manual trend log meter functionality

A manual trend log can be created with initial meter settings. The manual trend log supports the meter change command and meter consumption calculation. You can view the last meter change information on the manual trend log object. For more information, see Meter Function .

  • Trend Log Types
  • Creating a Manual Trend Log
  • Configuring a Manual Trend Log
  • Trend Units
  • Log Record Storage
  • Meter Function
  • Manual Trend Log Properties – Basic Tab
  • Manual Trend Log Properties – Meter Info Tab
  • References Tab
  • Extended Trend Logs