earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, AS-P, Virtual Project Servers
Functionalities: Localization
Product version: 3.2
10/15/2020

Manually Changing the SmartX Server Time and Date

You manually adjust the SmartX server clock when you configure or commission a SmartX server. When the SmartX server is running on a fully commissioned site it is important that you use a network time server to avoid drifting time in the SmartX server.

Note:
  • The Date & Time view displays the local time in the perspective of the SmartX server time zone settings and not in the perspective of WorkStation.

Show More
action_close

​To adjust the SmartX server time, time zone, and DST, you have to access the SmartX server through a WorkStation.

When adjusting the server clock, you can either set the time manually or you can refer to a network time server that automatically synchronizes the clock. Manual adjusting is used when you configure or commission a SmartX server. When the SmartX server is running on a fully commissioned site, it is important that you use a network time server to avoid drifting time in the SmartX server.

Beside predefined time zones, you can also customize the SmartX server time zone settings.

When adjusting the SmartX server time through WorkStation, it is the SmartX server operating system clock you adjust. The EcoStruxure Building Operation software has a transparent layer above the SmartX server operating system which manages the information about the time zone and DST time offset.

 
action_zoom_plus_stroke  The SmartX Server uses the operating system clock to which the EcoStruxure Building Operation software adds the time zone offset and DST
Figure: The SmartX Server uses the operating system clock to which the EcoStruxure Building Operation software adds the time zone offset and DST

Instead of configuring the time of each SmartX server, you can create a lead and shadow relationship that makes it possible to configure several SmartX servers through a single Enterprise Server.

To manually change the SmartX server time and date
  1. ​In WorkStation, in the System Tree pane, select the SmartX server you want to configure.

  2. Click the Control Panel tab.

  3. ​Click Network time and time zones .

  4. In the SmartX server Date & time view, select Manually adjust date & time .

  5. In the Local date & time boxes, enter the date and time of the SmartX server.

  6. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Network Time
  • Time and Time Zone Configuration in SmartX Server
  • Control Panel Tab
  • SmartX Server – Date & Time View
  • Synchronizing the SmartX Server Clock
  • Changing the Time Zone of an EcoStruxure BMS Server
  • Creating a Custom Time Zone of an EcoStruxure BMS Server