earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-C, AS-B, AS-P, Project Configuration Server, Project Configuration Tool
功能: 本地化
产品版本: 1.8
2016/10/13

Manually Changing the SmartStruxure Server Device Time and Date

You manually adjust the SmartStruxure server device clock if it is not synchronized with a network time server.

注释:
  • The Date & Time view displays the local time in the perspective of the SmartStruxure server device time zone settings and not in the perspective of WorkStation.

显示更多
action_close

​To adjust the SmartStruxure server device time, time zone, and DST, you have to access the SmartStruxure server device through a WorkStation.

When adjusting the server clock, you can either set the time manually or you can refer to a network time server that automatically synchronizes the clock. Beside predefined time zones, you can also customize the SmartStruxure server device time zone settings.

When adjusting the SmartStruxure server device time through WorkStation, it is the SmartStruxure server device operating system clock you adjust. Building Operation has a transparent layer above the SmartStruxure server device operating system which manages the information about the time zone and DST time offset.

 
action_zoom_plus_stroke  The Automation Server uses the operating system clock to which Building Operation adds the time zone offset and DST
图: The Automation Server uses the operating system clock to which Building Operation adds the time zone offset and DST

Instead of configuring the time of each SmartStruxure server device, you can create a lead and shadow relationship that makes it possible to configure several SmartStruxure server devices through a single Enterprise Server.

To manually change the SmartStruxure server device time and date
  1. ​On the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the SmartStruxure server device.

     
    action_zoom_plus_stroke
  3. ​Click Network time and time zones .

  4. In the SmartStruxure server device Date & time view, select Manually adjust date & time .

     
    action_zoom_plus_stroke
  5. In the Local date & time boxes, enter the date and time of the SmartStruxure server device.

  6. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Network Time
  • Time and Time Zone Configuration in Automation Server
  • SmartStruxure Server Device – Date & Time View
  • Synchronizing the SmartStruxure Server Device Clock
  • Changing the Time Zone of a SmartStruxure Server
  • Creating a Custom Time Zone of a SmartStruxure Server