You manually configure the trend chart y-axis to have a fixed scale. The trend chart has two y-axes, one to the left and one to the right. You can use this procedure to scale both axes.
In WorkStation, in the System Tree pane, select the trend chart you want to configure.
On the Trend Chart toolbar, click the Open trend chart settings button
Clear Auto scale left y-axis and Auto scale right y-axis .
In the Left y-axis minimum and Right y-axis minimum boxes, type the minimum value of the y-axis.
In the Left y-axis maximum and Right y-axis maximum boxes, type the maximum value of the y-axis.
Click OK .
The y-axis is now set with a fixed scale.