Funktionaliteter: Larm, Grundläggande funktionalitet, Trender
Produktversion: 2024, 7.0
2024-12-02

Mass Create Unit Management

You can only mass create alarms with identical units or no unit. When you mass create trend logs, each trend log gets the same unit as the logged variable.

 
action_zoom_plus_stroke Objects and properties with no unit are given the unit that is defined for the other objects.
Figur: Objects and properties with no unit are given the unit that is defined for the other objects.
  • Unit of Measure in Alarms
  • Trend Units
  • Mass Create
  • Units