You mass create alarms to create identical alarms for different objects, instead of creating the alarms one by one.
In Workstation, in the List View, select the objects that you want to create alarms for.
On the File menu, point to New and then click Alarm .
In the Create Object wizard, in the object type list, select the alarm type you want to create.
In the Prefix box, type a label that is added in front of the name of the alarms.
In the Suffix box, type a label that is added after the name of the alarms.
In the Description box, type a description for the alarms.
In the Destination box, enter the destination where you want to create the alarms. If you use A different folder, relative to the selected object , this destination applies to the first object in the list, and its path will work as a pattern for the relative path that is applied to all the remaining objects.
If the specified relative path pattern leads to an unavailable position for any of the objects in the list, Next and Create are disabled.
If you use A different folder, relative to the selected object , verify that the additional two lines show the resulting relative path pattern that you intend, and the way this pattern applies to an example object in the list.
Click Next .
See the alarm procedures for detailed information on how to create and set up your specific alarm type:
有关更多信息,请参阅 Creating a Multistate Alarm .
有关更多信息,请参阅 Creating a Variable Status Alarm .
有关更多信息,请参阅 Creating an Enumeration Alarm .
有关更多信息,请参阅 Creating a Matching Text String Alarm .
有关更多信息,请参阅 Creating an Out of Range Alarm .
有关更多信息,请参阅 Creating an Out of Reference Range Alarm .
有关更多信息,请参阅 Creating a Change of State Alarm .